Multiple STLink, one for each Project in STM32CubeIDE
Trying to have multiple ST-Link connected at one time.
Not working like I hoped.
Anyone got it working? (Multiple projects each with own STLink, all connected at same time)
Using STM32CubeIDE v1.6.1
---- My results ----
I try to set each project to a specific STLink Serial Number (I have 5 modules interconnected, and that list is growing), using:
- Project > Right Click > Debug As > Debug Cofigurations... > Tab:Debugger
- [+]ST-Link S/N > Scan > Select the correct one > Apply > Close
- It works with one, but gets confused when I have more than one
I've written the serial number on each device by connecting one at a time and scanning for changes.
- I've noticed that the first serial number listed seems to be incorrect, as it is often for an STLink I've disconnected. ****This may be a bug****
---- Suggestion ----
ST-Link serial numbers should be:
- Shown on the Virtual disk that opens when you connect the USB to the STLink (maybe in Details.txt)
- Printed on the label (STLink/V3, STLink/Mini, etc.)
Paul