Skip to main content
Visitor II
August 8, 2019
Solved

Need Evaluation Kit for this controller STM32L452RCT6 . Is there any alternate Eval Board available?

  • August 8, 2019
  • 2 replies
  • 2190 views

Actually In our Company the Controller is using STM32L452RCT6 Before Getting A sample Design Board. I need to test with any Eval Board of STM32L4 Series. I Need Evaluation Kit for this controller STM32L4RCT6 Is there any alternate Eval Board available. Hope I am looking forward for your reply.

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    STM32Cube_FW_L4_V1.14.0\Projects\NUCLEO-L452RE\Applications\USB_Device\CDC_Standalone\readme.txt

    2 replies

    Graduate II
    August 8, 2019

    There are several STM32L4R (L4+) boards in EVAL, DISCO and NUCLEO formats. These would likely suffice as proxies, lacking any specific stated requirements.​

    LuckyAuthor
    Visitor II
    August 9, 2019

    Hi Clive,

    Thank you for your response. As per our requirements the above 3 boards won't suitable , it doesn't have USB device support. The above reference Board support only USB OTG 2.0 FS. I need the Board with USB Device Support. Is it Board Available in Market with USB Device support. Hope I am looking forward for your reply.

    Graduate II
    August 9, 2019

    First, there is no such a STM32L4RCT6 MCU. Second, how about reading at least first lines in a data sheet?

    The devices embed an USB OTG full-speed device/host/OTG peripheral with integrated transceivers. The USB OTG FS peripheral is compliant with the USB 2.0 specification and with the OTG 2.0 specification.

    LuckyAuthor
    Visitor II
    August 9, 2019

    Hi Piranha,

    Thank for your response. I am extremely sorry spell mistake STM32L4RCT6 MCU instead of STM32L452RCT6 MCU.

    Actually, I am asking instead of a USB OTG full speed ,is it directly USB FS Device mounted on PCB Eval Board available or not.

    Graduate II
    August 9, 2019

    Pretty sure these can be HOST or DEVICE, if that's what the question is. Look at board code examples in CubeL4.

    Edit suggests a non L4+ device.​