New Custom STM32H743BI board PCB ST-Link "Error: No STM32 target found" ? Need Help!
Hi Everyone,
Hope you are doing well.
I am not able to connect my new custom board based on STM32H743BI with STM32CubeProgrammer using STLINK-V3SET. and get the "Error: No STM32 target found" when i try to connect.
As suggested in different threads i have confirmed the following:
- Reset is pulled high
- Boot0 is pulled low
- VDD is stable at 3..28V at all desired pins of the board
- VCAP 1&2 connected to 2.2uF capacitors showing voltage of 1.01V.
- VDDA is 3.28V, VSSA is Grounded,
I am using a 10 pin SWD connector.
The Circuit diagram is shown below



Thanks,