Skip to main content
Explorer
December 17, 2025
Question

No CDC ACM/COM port is being formed for USB Device code for STM32U5G-DK1

  • December 17, 2025
  • 2 replies
  • 35 views

Hello,

I am making a new project by importing the .ioc file of example code "Ux_Device_CDC_ACM" of STM32U5G-DK2. All the .c files of USB_stack and Azure_RTOS are also copied from the example project. Both, example project and My project, look same. My project builds also successfully. But no COM/ACM port is being formed after loading the project to STM32U5G-DK1 whereas, COMM port is being formed with Example project. 

What can be the reason ? Please help.

NOTE: USB Device mode Example project in repository is provided for STM32U5G-DK2 and not for DK1. So. we are trying to make a USB Device code by referring to this DK2 example.

 

With regard,

Sudarshan Chaudhary

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    December 18, 2025

    Hi @Sudarshan 

    I suggest performing a thorough debug to check errors during execution. Additionally, I noticed that the VDD core voltage differs in the schematics; please ensure that the power supply and related hardware implementation are correctly configured.

    SudarshanAuthor
    Explorer
    December 22, 2025

    USB ACM port is being formed now in my created project for USB CDC.

    But as soon as we enable USART3 in this project and call HAL_UART_Receive_IT() for USART3 on DK1 board in "main.c" file, just before "MX_ThreadX_Init()" ,  formed ACM port disappears and we are no longer able to send any data to DK1 board over USB. We have tried this with different USART3 NVIC priorities.

    I need to enable this USART3 for another thread.  If I comment HAL_UART_Receive_IT() from main.c and calls it inside the my UART related thread then ACM port forms but data transmission over USB gets stuck. I am unable to debug how and why USART3 is interfering with USB of STM32U5G9NJ-DK1.

    This above behaviour persists even with the "Ux_Device_CDC_ACM" example code of STM32U5G-DK2 board.

    Attached herewith is the screenshot of NVIC priorities in my program.