No ST-LINK detected on STM32F4-Discovery on Arch Linux
I'm trying to work with a STM32F4-Discovery board, and previously it connected perfectly okay, but a couple weeks ago something, seemingly out of nowhere, broke and CubeIDE stopped detecting the board and writing programs to it showing this message:

I tried reinstalling the IDE, downgraging the toolchain, upgrading the IDE, creating a fresh project and so on.
I'm running version 1.19.0 CubeIDE, using EndeavourOS (Arch-based).
Here are my udev rules for a relevant device:
# stm32 nucleo boards, with onboard st/linkv2-1
# ie, STM32F0, STM32F4.
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374b", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv2-1_%n"
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="3752", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv2-1_%n"My user is a member of the plugdev group.
But the important detail is that if I run stm32cubeide_wayland as root through sudo it is able to detect the board. (Still doesn't run the project, but that's because I don't have it setup for root either way.)
Edit:
Here's how it looks when I run stm32cubeide_wayland as root user:


While not root STLinkUpdate gives this:

And trying to run it gives the aforementioned ST-LINK firmware verification.