No STM32 Found on ST Link V2 JTAG Port
Before ST started bricking counterfeit st link V2 units, I was able to program my board without issue. I bought a confirmed genuine ST Link V2 from RS components and connected it exactly as shown, but it never connects to the target and all I can get is this output or an error which says no target found. I managed to upgrade the ST link firmware so it is connecting to the PC normally.
23:34:26:388 : STLinkUSBDriver.dll loaded
23:34:26:394 : STLinkUSBDriver.dll loaded
23:34:26:394 : ST-LINK SN : 37FF6C0630484B3838261443
23:34:26:394 : ST-LINK FW : V2J38S7
23:34:26:394 : Board : --
23:34:26:394 : Voltage : 1.05V
23:34:26:395 : Error: ST-LINK error (DEV_TARGET_CMD_ERR)
23:34:26:410 : Disconnected