"No STM32 target found" on consumer device
I'm trying to use a ST-LINKv2 to re-program a consumer device that I know has an STM32 of some kind inside (fairly sure it's a STM32L-something). I found four headers on the board that a continuity tester has shown to be Vdd, Vcc, SCLK, and SWDIO.
Connecting with only those 4 wires did not allow STM32CubeProgrammer to connect to the device. It gives the message "No STM32 target found!". Same with the ST-Link Utility. So I next tried tying boot0 high (w/ and w/out a 1k resistor). I have confirmed that this prevents the device's normal program from starting. Connection still fails. I then tried connecting NRST to the ST-LINK so that it could control hardware-reset. I can verify that trying to connect to the device does reset it over NRST. But it still can't connect
Port: SWD
Frequency: 100kHz
Mode: Under reset
Reset mode: Hardware Reset
Output:
12:57:17 : ST-LINK SN : 55FF6E066684564922161687
12:57:17 : ST-LINK FW : V2J37S7
12:57:17 : Board : --
12:57:17 : Voltage : 1.05V
12:57:17 : Error: No STM32 target found!If I increase the frequency to 4000kHz, then the error changes to: "Error: ST-LINK error (DEV_TARGET_CMD_ERR)"
I've tried so many combinations of configurations, swapped the CLK/IO pins just to be sure, updated the ST-LINK firmware, but nothing fixes the connection. Am I missing something obvious here? Is it possible that the chip is locked-down during manufacturing so that it can't be modified?