No STM32 target found - STM32L486 sanity check
I've recently put together a new design and ST-Link doesn't seem to detect the STM32L486 on the board using the STM32CubeProgrammer
The part used is the 144 LQFP version, but I've double checked the pins and connections for the SWD port. I'm supplying the microcontroller with 3.3V, but powered up is sitting at 3.2V strangely. Strangely I'm noticing some shorts from other pins to the 3v3 rail from some GPIO pins (PA2, PF2, PF11) and I'm not sure if this is normal when the device is unpowered.
Does anyone have any idea what might be the problem here? Schematic below