No voltage on ST-Link v3 Minie BTB T_VCC (10) pin
Dear All,
Just now I have plugged my ST-Link v3 Minie in. Updated it via CubeIDE. All looks good.
I might have overseen something (scanned the user manual), but the BTB (CN2) connector on my ST-Link v3 Minie gives 0V voltage between T_GND(6) and T_VCC (10) on the bottom side.
I was expecting something around 3.3V.
Or does my target board need to supply this voltage? Did I miss something? Solder Bridge?
Help is much appreciated.
Ps: CN4 STDC14 gives 2.7V on pins 3 and 1.