Not getting uart Interrupt
Hi,
Im doing a project where uart is configure in interrupt method to receive 5 bytes.For this I'm using stm32h743 mcu.Im facing an issue with the uart reception.As mentioned above i expected to get an interrupt after receiving 5th byte if of the packet, in that case its working finebut when i try to seng 8bytes of data im getting an interrupt for the very first time in that case after that im not getting any interrupt. On that that in used to get an hal ok from the "HAL_UART_Receive_IT". How can i fix this , could some one help me out.Thanks in advance.