NRST / Reset Pin in STM32H7 more ESD sensitive than in STM32F4?
Hi,
I have a new PCB here which somehow has latch up problems on the NRST pin quite recently. Usually then the NRST pin would just have zero DC resistance (or typically 1 Ohm) to GND. And then of course also the oscillator (8MHz XTAL) will not start working and chip keeps in reset (this is then also the error message of ST-LINK).
I use an external 10kOhm resistor against 3V3 (VCC) and then I have an about 5cm long PCB trace to the 4pin ST-LINK Debug connector... .
In the last 3 weeks I had about 5 times such a latch up problem with this PCB (STM32H750 processor, 100pin LQFP, "Y" version - this is still the startup version I think according to errata sheet...).
Now I added a 100nF capacitor to the reset line against GND. Hoping that it will be fixed now (Nucleo H743 also has such a cap, and in the datasheet they recommed it if a reset button is installed ... I do NOT have a reset button in my PCB, but maybe this cap anyhow somehow much better ... just I never had to do this with STM32F4 PCBs ... and also I never had any STM32 latchup problems before ... this is my first STM32H7 PCB...).