Nucleo 144 STM32H7 ESD protection
Hello!
I have a question about ESD protection of Nucleo 144 STM32H7 development board. As I've noticed from the schematics the board uses ESDA7P60, ESDALC6V1, USBLC6-2SC6 and USBLC6-4SC6 for ethernet, buttons, SWD connectors and USB.
Isn't it easier and more convenient to use one part in all these cases, for example USBLC6-4SC6? It suits ethernet, it also can be used for USB (just left 2 other channels not connected).
And is there any reason why USBLC6 cannot be used for user buttons or for external PLS connectors (SPI, UART, GPIOs' signals etc)?
Thanks in advance.