Skip to main content
Graduate
December 7, 2024
Solved

Nucleo C031C6 Virtual COM Port problem

  • December 7, 2024
  • 3 replies
  • 1046 views

I am working on the Nucleo C031C6 and struggling to use the virtual com port. The datasheet says that the virtual com port is connected to PA3 and PA2, so I want to send data to my computer with USART2. Unfortunately, I do not understand why the pins allocated are orange, and I can't access usart 2: it is in grey and permanently disabled. I do not get the problem

 

Capture d’écran 2024-12-07 à 12.46.09.pngimage.png

 

 

 

 

    This topic has been closed for replies.
    Best answer by MM..1

    You require init right way

    MM1_0-1733573828290.png

    i click this and all is green

     

    3 replies

    MM..1Answer
    Graduate II
    December 7, 2024

    You require init right way

    MM1_0-1733573828290.png

    i click this and all is green

     

    Super User
    December 8, 2024

    Pins colored orange mean that the pins are assigned a function, but the corresponding component is not enabled in the left side (Categories). In your case the USART2 is not enabled or not in the correct mode. Same about the debugger pins.

    ST Employee
    December 9, 2024

    Attache is NUCLEO-C031C6 ioc file.