Nucleo F103RB run on startup
Hi,
I'm going to say that this is a really nooby question, however I cannot find the answer anywhere.
Background, I'm using a nucleo F103RB, and I've programmed it using CubeIDE. I can connect the board, debug and run the program fine. The board is powered via Vin at the correct voltages, with JP1 disconnected and JP5 set to E5V.
I need to be able to run this program immediately after the board powers on, without a USB connection. How do I upload a release build of my program to it, because whenever I try using cubeprogrammer, it doesn't run the program after it has restarted. When I've tried dragging and dropping the .elf file in, it's given me a write error.
Thanks in advance for your help,
P