Skip to main content
Graduate
June 14, 2024
Solved

Nucleo-F767ZI must reset after power ON

  • June 14, 2024
  • 1 reply
  • 2473 views

Hello everyone, my programme on Nucleo-F767ZI do not run when I power ON by external power supply. I force to press reset button or power supply st-link by usb cable.

I searched some solutions such as: BOOT0 to GND; or turn on bit POR = 1 in RCC_CSR, but nothing worked. 

I don't want to use external circuit to reset.

Anyone can share with me some useful solutions to solve this issue?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    So can I remove SB3 and SB111 like 3.3V?


    No, so you need to read the first section (VIN/E5V) and apply the described power sequence procedure.

    1 reply

    Super User
    June 14, 2024

    Hi,

    so your nucleo is running, if connecting st-link -> USB ?

    But without power on st-link - not ?

    Then look , what you get, if st-link not powered:

    AScha3_0-1718345216792.png

    Clk is coming from st-link , so you have to power the st-link, to get the 8MHz clk, 

    or set solder bridges + a crystal connected to F767,

    or use only internal HSI clk in your program.

    +

    Boot0 at gnd , is always needed, if you dont want to start the internal bootloader.

    +

    NRST has to be separated from st-link, if you dont power it; so power st-link, even if you dont use it - 

    or separate the F767 reset from not powered st-link.

    Just look at the circuit of your board, to see, what to do .

    https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

     

    ManhPhamAuthor
    Graduate
    June 14, 2024

    Thanks for your advice.

    Using clk HSI make the timer run incorrectly in my programme. Best option is supply power for st-link, I don't want to supply through the Micro USB port. 

    Could I external supply power for st-link by jumper or other pin ? Which pin, pls help?

    Technical Moderator
    June 14, 2024

    Hello,

    Please refer to the UM1974 page 23:

    SofLit_0-1718358483613.png

    For 3.3V power supply: you need to remove SB3 and SB111 to disconnect ST-LINK from the main MCU because it's keeping resetting it.