NUCLEO-F767ZI unable to do a FullChipErase
Hi,
i was playing with OptionBytes on my custom USB-Bootloader and... I end up in a bricked NUCLEO board... the CPU itself is still running (I can even update an application) but I cannot connect via ST-LINK and/or DfuSe anymore...
The error message is:
09:12:27 : Can not connect to target!
If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
09:12:28 : No target connected
On the device folder:
DETAILS.TXT
------------------
Version: 0221
Build: Sep 18 2018 11:09:21
FAIL.TXT
------------
The interface firmware FAILED to reset/halt the target MCU
ST-Link utils is v4.3.0.0
ST-LinkUSB-Driver is v5.1.0.0
ST-Link CLI is v3.3.0.0
The option "connect under reset" & pressing the B2 (reset) button before doing a chip erare seems not to work... somewhere there is a note regarding SB111 (pad between NRST-RST) but in my case a 0 ohm resistor is already there.
Any ideas on how to unbrick my NUCLEO board ?
thanks,
Giampaolo