Nucleo-H563ZI as USB host?
Hello,
I would like to know if Nucleo-H563ZI board could be used as a USB host, using the user USB (CN13). I'm asking because I'm a bit confused, honestly - I've only found examples where it's being used as a device and the board manual seems to mention only as device and sink only for the CN13 connector. OTOH, in CubeIDE, after starting a new project based on this board, the USB and USBX can be configured as host, without any restriction. And, if it's possible, should UCPD1 and USBPD be enabled along with USB and USBX, or it's enough to call HAL_PWREx_EnableVddUSB at the end of HAL_HCD_MspInit?
Basically, what I want to implement is reading VID, PID and SN from a USB storage device plugged in CN13 and printing them over USART3.
Thanks!