Skip to main content
Visitor II
September 24, 2025
Solved

Nucleo-H563ZI shows a constant 660mV on DAC output in idle state

  • September 24, 2025
  • 3 replies
  • 757 views

Hi,

I am working on DAC on Nucleo-H563ZI board. I am using PA4 on ST Morpho header as DAC1_OUT1.

In idle state when the USER USB port is connected (irrespective of ST-LINK port connection), it shows a constant voltage of 660mV on output.

Nucleo_H563_USB_660mv_DAC.jpg

nagahimanshu7_0-1758705383826.png

During sine generation using DAC, there is no offset of this voltage observed and the output is in range.

nagahimanshu7_1-1758705437112.png

But if the USER USB is not connected, the output remains 0V. What could probably be causing the 660mV idle state output?

    This topic has been closed for replies.
    Best answer by AScha.3

    Hi,

    from circuit of Mb1404 , PA4 is connected to VBUS_SENSE .

    AScha3_0-1758708457942.png

    +

    AScha3_1-1758708574182.png

    So open SB56 , if you dont want to use vbus-sense or need "free" PA4.

    3 replies

    Super User
    September 24, 2025

    Have you checked the schematics?

    eg, is there anything connected to that pin related to the User USB?

    AScha.3Answer
    Super User
    September 24, 2025

    Hi,

    from circuit of Mb1404 , PA4 is connected to VBUS_SENSE .

    AScha3_0-1758708457942.png

    +

    AScha3_1-1758708574182.png

    So open SB56 , if you dont want to use vbus-sense or need "free" PA4.

    Visitor II
    September 24, 2025

    Hi @Andrew Neil @AScha.3 

    Thanks for the inputs.

    Super User
    September 24, 2025

    You're welcome.

    Always important to check the board schematics!