Skip to main content
Visitor II
July 4, 2020
Question

NUCLEO-H743ZI2 and STLink VCP

  • July 4, 2020
  • 2 replies
  • 1670 views

Hi,

Can someone throw some light in here, please ?

I have a Nucleo-H743ZI2 (MB1364C) board. From schematics it appears to me that UART3 is connected to STLink and can be used as a regular COM port ?

Is it possible to use UART3/VCP on the STLink as a regular serial port ?

Running Putty on COM8 STLink Virtual COM port, I get some chinese chars

0693W000001s9wfQAA.png

Any idea, what's going on ?

Are those coming from the STLink firmware ?

The code that I am running on it:

#include "main.h"
 
/**
 * System Clock Configuration
 * The system Clock is configured as follow :
 * 	System Clock source	= PLL1 (HSE BYPASS)
 *	SYSCLK(Hz)		= 400000000 (CPU Clock)
 *	HCLK(Hz)		= 200000000 (AXI and AHBs Clock)
 *	AHB Prescaler		= 2
 *	D1 APB3 Prescaler	= 2 (APB3 Clock 100MHz)
 *	D2 APB1 Prescaler	= 2 (APB1 Clock 100MHz)
 *	D2 APB2 Prescaler	= 2 (APB2 Clock 100MHz)
 *	D3 APB4 Prescaler	= 2 (APB4 Clock 100MHz)
 *	HSE Frequency(Hz)	= 8000000
 *	PLL_M			= 4
 *	PLL_N			= 400
 *	PLL_P			= 2
 *	PLL_Q			= 4
 *	PLL_R			= 2
 *	VDD(V)			= 3.3
 *	Flash Latency(WS)	= 4
 */
static void SystemClock_Config(void)
{
	/* Power Configuration */
	LL_PWR_ConfigSupply(LL_PWR_LDO_SUPPLY);
	LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE1);
	while (LL_PWR_IsActiveFlag_VOS() == 0) { }
 
	LL_RCC_HSE_EnableBypass();
	LL_RCC_HSE_Enable();
	while (LL_RCC_HSE_IsReady() != 1) { }
 
	LL_FLASH_SetLatency(LL_FLASH_LATENCY_4);
 
	/* Main PLL configuration and activation */
	LL_RCC_PLL_SetSource(LL_RCC_PLLSOURCE_HSE);
	LL_RCC_PLL1P_Enable();
	LL_RCC_PLL1Q_Enable();
	LL_RCC_PLL1R_Enable();
	LL_RCC_PLL1FRACN_Disable();
	LL_RCC_PLL1_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_2_4);
	LL_RCC_PLL1_SetVCOOutputRange(LL_RCC_PLLVCORANGE_WIDE);
	LL_RCC_PLL1_SetM(4);
	LL_RCC_PLL1_SetN(400);
	LL_RCC_PLL1_SetP(2);
	LL_RCC_PLL1_SetQ(4);
	LL_RCC_PLL1_SetR(2);
	LL_RCC_PLL1_Enable();
	while (LL_RCC_PLL1_IsReady() != 1) { }
 
	LL_RCC_SetSysPrescaler(LL_RCC_SYSCLK_DIV_1);
	LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
	LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_2);
	LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);
	LL_RCC_SetAPB4Prescaler(LL_RCC_APB4_DIV_2);
	LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);	/* Set PLL1 as System Clock Source */
	while (LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL1) { }
 
	SysTick_Config(400000000 / 4000);			/* Set systick to 1ms */
	SystemCoreClock = 400000000;				/* Update CMSIS variable */
}
 
#define STLINK_RX_Pin		LL_GPIO_PIN_8
#define STLINK_TX_Pin		LL_GPIO_PIN_9
#define APB_Div			2
 
void config_usart(void)
{
	LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOD);
 
	LL_GPIO_SetPinMode(GPIOD, STLINK_TX_Pin, LL_GPIO_MODE_ALTERNATE);
	LL_GPIO_SetAFPin_8_15(GPIOD, STLINK_TX_Pin, LL_GPIO_AF_7);
	LL_GPIO_SetPinSpeed(GPIOD, STLINK_TX_Pin, LL_GPIO_SPEED_FREQ_HIGH);
	LL_GPIO_SetPinOutputType(GPIOD, STLINK_TX_Pin, LL_GPIO_OUTPUT_PUSHPULL);
	LL_GPIO_SetPinPull(GPIOD, STLINK_TX_Pin, LL_GPIO_PULL_NO);
 
	LL_GPIO_SetPinMode(GPIOD, STLINK_RX_Pin, LL_GPIO_MODE_ALTERNATE);
	LL_GPIO_SetAFPin_8_15(GPIOD, STLINK_RX_Pin, LL_GPIO_AF_7);
	LL_GPIO_SetPinSpeed(GPIOD, STLINK_RX_Pin, LL_GPIO_SPEED_FREQ_HIGH);
	LL_GPIO_SetPinOutputType(GPIOD, STLINK_RX_Pin, LL_GPIO_OUTPUT_PUSHPULL);
	LL_GPIO_SetPinPull(GPIOD, STLINK_RX_Pin, LL_GPIO_PULL_NO);
 
	LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_USART3);
	LL_USART_Disable(USART3);
 
	LL_USART_SetTransferDirection(USART3, LL_USART_DIRECTION_TX_RX);
	LL_USART_ConfigCharacter(USART3,
				 LL_USART_DATAWIDTH_8B,
				 LL_USART_PARITY_NONE,
				 LL_USART_STOPBITS_1);
 
	LL_USART_SetHWFlowCtrl(USART3, LL_USART_HWCONTROL_NONE);
	LL_USART_SetOverSampling(USART3, LL_USART_OVERSAMPLING_16);
	LL_USART_SetBaudRate(USART3,
			 SystemCoreClock/APB_Div,
			 LL_USART_PRESCALER_DIV1,
			 LL_USART_OVERSAMPLING_16,
			 115200);
 
	LL_USART_SetTXFIFOThreshold(USART3, LL_USART_FIFOTHRESHOLD_1_8);
	LL_USART_SetRXFIFOThreshold(USART3, LL_USART_FIFOTHRESHOLD_1_8);
	LL_USART_DisableFIFO(USART3);
	LL_USART_Enable(USART3);
 
	while ((!(LL_USART_IsActiveFlag_TEACK(USART3))) ||
	 (!(LL_USART_IsActiveFlag_REACK(USART3)))) { }
}
 
 
uint8_t bytes = 0;
const uint8_t tx_str[] = "STM32H743 USART Tx Test: @115200bps, 8N1\r\n";
 
void BufferTransfer(void)
{
	/* Send characters one per one, until last char to be sent */
	while (bytes < sizeof (tx_str)) {
		while (!LL_USART_IsActiveFlag_TXE(USART3)) {}	/* Wait for TXE flag to be raised */
 
		if (bytes == (sizeof (tx_str) - 1))
			LL_USART_ClearFlag_TC(USART3);		/* If last char to be sent, clear TC flag */
 
		LL_USART_TransmitData8(USART3, tx_str[bytes++]);
	}
	while (!LL_USART_IsActiveFlag_TC(USART3)) {}		/* Wait for TC flag to be raised for last char */
}
 
 
int main(void)
{
//	SCB_EnableICache();
//	SCB_EnableDCache();
	SystemClock_Config();
	config_usart();
	BufferTransfer();
 
	while (1) { }
}

    This topic has been closed for replies.

    2 replies

    Graduate II
    July 4, 2020

    >>Any idea, what's going on ?

    Clocks/baud rate not what you want. Suspect you're going to need to unpack the register settings, and determine what you have. Scope the TX pins to measure bit timing achieved.

    Attached code outputting at 115200 8N1, should prove the plumbing and terminal working.

    Visitor II
    July 4, 2020

    Hi Clive,

    Thanks for the quick reply and the help.

    As you rightly said, the clocks issue and not setting the clock source.

    These 2 changes helped.

    #define APB_Div         4

    LL_RCC_SetUSARTClockSource(LL_RCC_USART234578_CLKSOURCE_PCLK1);      /* Clk source */

    Though that did the trick, still the question about the Chinese chars.

    If I do comment out the clock source, I still do see the chinese chars.

    0693W000001s9zoQAA.png

    Any thoughts ?

    Thanks,

    Manu

    Visitor II
    July 4, 2020

    I did try a Google translate of the characters,

    昀▒▒昆▒▒▒▒▒▒▒▒▒▒

    Yún ▒▒kūn ▒▒▒▒▒▒▒▒▒▒

    It seems to read as Yun and Kun ?? meaning Cloud and Earth/Universe ??

    But still wonder where they come from ..

    Thanks,

    Manu

    Super User
    July 4, 2020

    Is there an external pullup on that line? Line could be toggling due to noise or interference when the chip is in reset.

    If you got those chars when your baud settings were incorrect then it's probably not from something your chip is doing.

    I suppose the ST-Link chip could be creating those. Seems odd though.

    Visitor II
    July 4, 2020

    No pullups on the line.

    I also wondered why ST Link was doing it, but had no clue.

    My bad, it was not commenting out the clk source, that brought out those chars, but change to the baud rate with:

    #define APB_Div         4

    to

    #define APB_Div         2

    That clears up the issue, I guess ..

    Thanks and sorry about the noise.