Skip to main content
Visitor II
November 14, 2025
Solved

NUCLEO H753Z: ST Link V3

  • November 14, 2025
  • 3 replies
  • 501 views

Hello everyone,

I am using the NUCLEO H753ZI microcontroller it has ST Link V3 can i debug this board with the ST Link can you tell me what version of ST do i need to get to debug my board and also can you provied me the document for debugging with ST link.
                           Thank you

    This topic has been closed for replies.
    Best answer by mƎALLEm

    This is to use a printf over the serial wire viewer

    You can refer to this article: Using the ITM console for printf redirects and LWIP debug messages

    3 replies

    Technical Moderator
    November 14, 2025

    Hello @JhonVijay and welcome the the ST community,

    Not sure I understood the question. The on board STLINK-V3 is intended to connect to the on-board MCU in your case: STM32H753 MCU.

    You can use it with STM32CubeIDE for debug, you can use it with STM32CubeProgrammer to upload, read to/from the internal or (if available) an external flash.

    You can also refer to the board's user manual UM2407 / section 7.3 Embedded STLINK-V3E

    JhonVijayAuthor
    Visitor II
    November 14, 2025

    I had debugged my Nucleo board with the J Link with the segger RTT. Now i like to change to STLINK So l would like to know what version of ST external debuger support my board which can be used for debuging my device

    Technical Moderator
    November 14, 2025

    You can connect a J-LINK on CN5 connector on NUCLEO H753ZI:

    mALLEm_0-1763121074179.png

    Please refer to the user manual of the board UM2407 / section 7.3.3 Using an external debug tool to program and debug the on-board STM32H7

    For STLINK you can use the external version STLINK-V3 (I don't know what the reason to use an external version while there is one on board)

    Hope that does answer your question

     

    JhonVijayAuthor
    Visitor II
    November 14, 2025

    Thank you @mƎALLEm  The thing is i had tryied to debug using the internal debugger to print the debugging messages by refering this vedio but i couldn't see the any debug messages so i wanted to try the external STLINK.Can you please proveide any documentation on debuging with the internal STLINK 

    Technical Moderator
    November 17, 2025

    @JhonVijay This is not the right post to accept. I will unmark it and select the one that answered your original question.

    mALLEm_0-1763370619686.png