NUCLEO-H753ZI ADC channel Pins location - Can those pins be accessible on this board
Hi,
Refer to NUCLEO-H753ZI's schematics - mb1364-h753zi-c01_schematic.pdf
1. About 8 ADC channels go to CN11 and CN12 on this schematics without the pin numbers denoted..
Do all pins on the connectors CN11 and CN12 accessible since there are no physical connectors?
2. PA0_C, PA1_C, PC2_C, PC3_C, PH2, PH3, PH4, PH5 are all ADC channels, but they are missing in the schematics. Why?
Below is what I found -
ADC1/2
.ADC12_INP0 PA0_C
.ADC12_INP1 PA1_C
.ADC1_INP2 PF11 CN9-11 PF10 DNF?
.ADC12_INP3 PA6 CN7-8
.ADC12_INP4 PC4* CN12 DNF MORPHO CONNECTOR RIGHT SIDE OPAMP1_VOUT, COMP1_INM
.ADC12_INP5 PB1 CN9-7 COMP1_INM
.ADC1_INP6 PF12 CN10-7 DNF PF4
.ADC12_INP7 PA7* CN12 DNF MORPHO OPAMP1_VINM
.ADC12_INP8 PC5* CN12 DNF MORPHO OPAMP1_VINM
.ADC12_INP9 PB0 CN10-31 OPAMP1_VINP, COMP1_INP
.ADC123_INP10 PC0 CN9-3
.ADC123_INP11 PC1 CN11
.ADC123_INP12 PC2 CN9-9 (SB53)
.ADC12_INP13 PC3 CN9-5
.ADC12_INP14 PA2 CN12
.ADC12_INP15 PA3 CN9-1
.ADC1_INP16 PA0 CN10-29 SB75 WKUP1
.ADC1_INP17 PA1 CN11
.ADC12_INP18 PA4 CN7-17 DAC1_OUT1
.ADC12_INP19 PA5 CN7-10 DAC1_OUT2
ADC2
.ADC2_INP2 PF13 CN10-9 DNF PF5
.ADC2_INP6 PF14 CN10-11 DNF PF6
ADC3
.ADC3_INP0 PC2_C
.ADC3_INP1 PC3_C
.ADC3_INP2 PF9 CN9-28
.ADC3_INP3 PF7 CN9-26
.ADC3_INP4 PF5 CN10-9 SB48 PF13
.ADC3_INP5 PF3 CN7-20
.ADC3_INP6 PF10 CN9-11 SB60 PF11
.ADC3_INP7 PF8 CN9-24
.ADC3_INP8 PF6 CN10-11 SB54 PF14
.ADC3_INP9 PF4 CN10-7 SB38 PF12
.ADC123_INP10 PC0 CN11
.ADC123_INP11 PC1 RTC_TAMP3/WKUP6
.ADC123_INP12 PC2 CN11
.ADC3_INP13 PH2 X
.ADC3_INP14 PH3 X
.ADC3_INP15 PH4 X
.ADC3_INP16 PH5 X