NUCLEO-H753ZI board's ADC1/2 ADC3 channel Index with GPI/O Pin assignments
Hi,
Could you list NUCLEO-H753ZI board's ADC1/2 ADC3 channel Index with GPI/O Pin assignment table with the connector name / pin index on the board, using channel number as the index
It is very difficult to configure CUBEMAX-ADC without this Table. Especially, some ADC pin(s) may not be accessible on this board. I appreciate if you can provide this table:
ADC1/2 Example
Channel Index GPIO NUCLEO Board Connector Index Connector Pin Index Sharing Info
IN3 PA6 CN8-D12 (Pin 7) with ADC3_IN12
ADC3 Example
Channel Index GPIO NUCLEO Board Connector Index Connector Pin Index Sharing Info
IN2 PA2_C CN8-A2 Pin 9 with ADC1/2_IN14
Thanks,
Rong