Nucleo-H755ZI-Q no longer programmable
This fault has appeared very abruptly. One hour ago I was working with the board just fine, programming via STM32CubeIDE. Then I swapped the board to a different USB port on my laptop, now it is not programmable.
When I hit the 'Run' button, it appears to be working, but then fails. The output is below:
STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61238
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
Log output file: C:\Users\tcarney\AppData\Local\Temp\STM32CubeProgrammer_a21416.log
ST-Link Server is running on port : 7184
ST-LINK SN : 004D00453532511331333430
ST-LINK FW : V3J15M6
Board : NUCLEO-H755ZI-Q
Voltage : 3.31V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a21416.srec
File : ST-LINK_GDB_server_a21416.srec
Size : 41.41 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.061
Verifying ...
Download verified successfully
Target no device found
Failed to restart ST-LINK connection
Failed to read DAP register for AP 3
Failed to read ROM table via AP 3
Failed to reinitialize device
Shutting down...
Exit.

As you can see, it looks as though it did program, but then failed to restart. I know that it is not working because I am monitoring the UART for expected output but nothing is coming out.
If I try to 'Run' again, I get

If I connect BT0 to VDD I can then connect to the board using STM32CubeProgrammer and do a full chip erase, but this just gets me back into the state where I started from. If I try to program the device from within STM32CubeProgrammer, I get this:

Once again, it seems to be programming, and then failing on restart.
I have updated to v1.16.0 of the IDE, and V3.J15.M6 of the STLink firmware, but nothing changes.
Can anyone offer any insight into what is happening or how I might fix it?
Thanks