NUCLEO-H7A3ZI: Possible to use all 3 DAC channels simultaneously?
In reading the manuals and datasheets, it seems like it should be possible to simultaneously use all 3 channels (DAC1 Channel 1, DAC1 Channel 2, and DAC2 Channel 1) of the onboard DACs at once, emitting separate values on each. However, no matter what I've done, I can't seem to get PA6 to do anything but float. PA4 and PA5, the DAC1 channels, both work exactly as expected, and both DACs are in the READY state, but PA6 never emits anything.
Happy to post any portion of the code or registers here but most of it is the standard Cube autogen.
This is with the NUCLEO-H7A3ZI-Q 144-pin board.