NUCLEO-H7A3ZI-Q are not working after few hours (no ST-link connection possible)
Hello all,
I would like to ask for your experience with NUCLEO-H7A3ZI-Q board. It is new board which started to be produced. I ordered 3 same boards. They were used at two workbenches independent.
All products have same behavior:
First 2-3 hours are working without any issue (during whole time, no external components connected, just USB port for debugging and power)
There was used just example from st.com supplier ...NUCLEO-H7A3ZI-Q\Examples\UART_TwoBoards_ComDMA, there was used Virtual Serial port....
I would like to note. There were not activated/deactivated any lock bits in processor just flashing example and debugging software + small modification in code for serial port
- There were used just debugging and flashing procedures. Board will stop to communicate by integrated ST-Link interface (after 2-3 hours). There is same behavior if external ST-Link v3 debugger is connected to the board which is not working with integrated ST-Link
- The same behavior was observed at two workbenches independently.
I expect that some of you can have similar experience. Maybe, there is some solution or procedure how to exchange boards for good one from the supplier (www.mouser.de). From my perspective, there is some production issue at least in the same production batch.
thank you in advance
Best regards
Julius