Nucleo MB1364 as standalone ST-Link V3
Hi there,
I have developed my project long time with MB1364E, exactly with H723ZG.
Now I have got my own PCB with H743. I would like to use ST-Link V3 (SWD) from Nucleo board just the same as it works for cuttable ST-Link from L4 Nucleos, e.g.:
https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-use-the-standalone-st-link-capability-of-my-nucleo-after/td-p/306461
I have removed JP4 "Idd measurement", JP2 "Power source selection" and JP5 "Power selection".
But it seems that Nucleo ST-Link is hardcoded to support only this board.
Log from CubeProgrammer:
07:59:18:504 : UR connection mode is defined with the HWrst reset mode
07:59:20:007 : ST-LINK SN : 003600453331510B33323639
07:59:20:007 : ST-LINK FW : V3J12M3
07:59:20:008 : Board : NUCLEO-H723ZG
07:59:20:008 : Voltage : 3.29V
07:59:20:008 : Error: ST-LINK error (DEV_TARGET_HELD_UNDER_RESET)
07:59:20:024 : Disconnected
However, when my PCB is not supplied I get another error from CubeProgrammer, the voltage is correctly 0.00V detected:
08:03:06:200 : UR connection mode is defined with the HWrst reset mode
08:03:06:234 : ST-LINK SN : 003600453331510B33323639
08:03:06:234 : ST-LINK FW : V3J12M3
08:03:06:235 : Board : NUCLEO-H723ZG
08:03:06:235 : Voltage : 0.00V
08:03:06:235 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
08:03:06:249 : Disconnected
Yes, I can still work with external ST-Link V3 and my board. But I also want to reuse part of not anymore used NUCLEO board.
Let's say, just to reduce garbage and save the world.
Is there a way to free the ST-Link V3 from NUCLEO board?