NUCLEO-U5A5ZJ-Q - USB port configured as host
Hi everyone. I have a problem with my U5A5ZJ-Q core board. The mounted microcontroller is STM32U5A5ZJT6QU. The project is to drive a QUECTEL em05 LTE modem. I need to configure the USB port exposed by PA11 and PA12 in Host mode. I am using the standard Host libraries in Middlewares and also the files in the USB_Host folder. I am trying to configure everything without success. I can't find exact written procedures to do this. Has anyone had problems? Has anyone tried? The problem is with the initialization of the USB Host port. It remains in reset mode and the CSRST bit never returns to 0. Below is a portion of the serial log that I printed on the monitor. " [CLK] Enabling HSI48...<CR><LF>
[CLK] HSI48 RDY=1<CR><LF>
[CLK] CLK48 <- HSI48 (via __HAL_RCC_CLK48_CONFIG)<CR><LF>
[USBH] Init...<CR><LF>
[LL] USBH_LL_Init (FS)<CR><LF>
[HCD] Enter HAL_HCD_Init<CR><LF>
[MSP] AFRH(GPIOA)=0x000AA770 AF_PA11=10 AF_PA12=10<CR><LF>
[MSP] GCCFG=0x02010000 GUSBCFG=0x00001400<CR><LF>
[HCD][PRE] GUSBCFG=0x00001400 GCCFG=0x00000000 GRSTCTL=0x80000000<CR><LF>
[HCD] Call USB_CoreInit<CR><LF>
[LL] USB_CoreInit (v6: FS-PHY pre-CSRST ON) enter<CR><LF>
[LL][DBG] pre-CSRST: GUSBCFG=0x00002800 GCCFG=0x02010000 GAHBCFG=0x00000000 GRSTCTL=0x80000000 GINTSTS=0x04000020<CR><LF>
[LL][ERR] CSRST timeout GRSTCTL=0x80000001<CR><LF>
[HCD][ERR] USB_CoreInit FAIL<CR><LF>
[LL] HAL_HCD_Init FAIL (FS)<CR><LF>
[USBH] USBH_Init OK (HOST_HS)<CR><LF>
[USBH] CDC class registered<CR><LF>
[USBH] Host started<CR><LF>
SYSCLK = 80000000 Hz<CR><LF>" I'm powering USB directly. Can anyone help me? Any advice or procedure? Has anyone used a different microcontroller that successfully implemented USB Host and perhaps driven an LTE modem? Thanks a lot.