Number of SPI clock cycles changes when below 1Mhz
Hi, I find that the number of SPI clock cycles change when I set the SPI clock speed below 1Mhz.
When SPI Clock > 1 Mhz, the SPI clocks out 8 cycles 4 times, as expected. ( I am sending 4 bytes of data)
When the SPI Clock < 1Mhz, the SPI clocks out 32 cycles despite transmitting only 4 bytes of data in the HAL function call.

What is the reason for the number of clock cycles to change despite only changing the SPI clock speed in the cubemx tool?