Question
Okay I have previously posted on this community and got great feedback. So I spent a while fixing my schematic for the STM32F722RET6. If someone could check my pin outs of VDD and VSS that would help a lot.
It's an ugly schematic I know. The reason It's so tight is because I'm planning on adding more components, like a gyroscope, barometer, etc. I am using the ST-links debugger. But I just need someone to help and check my VDD and VSS pinouts. Each VDD is connected to a 100nF capacitor and all of them are also connected to a 5.0uF tantalum capacitor and the VSS are connected to ground.