On board ST-LINK/v2 debugging on Nucleo-144 board (STM32H743) - upper flash banks show 0xFF, not real values.
- Keil MDK5 v5.31
- STM32H743
- Nucleo-144 board
- STlink Firmware: STM32 Debug+Mass storage+VCP V2.J35.M26
Bank 0 Sector 0 and 1 I can view in the memory windows
Bank 0 Sectors 2 through 7, as well as all as Bank 1, show up as 0xFF, i.e. I can't view their contents while debugging.
Went through section 3.5 FLASH protection mechanisms in the DM00314099.pdf
every thing looks like the default settings and OK.
The RDP 0 values do not appear to be set?
Question:
Is there some other setting that will let me look at the flash bank values? Or is this just a design limitation?