Skip to main content
Explorer
September 8, 2023
Question

On STLINK V3, Target Board does not run after proggramming...

  • September 8, 2023
  • 2 replies
  • 1563 views

Hi, I am suffer something troublesome.

I should press ResetButton then the TargetBoard runs.

on STLink V2.x, Target Board automatically runs after programming. (STM32L4xx / STM32F7xx)

I took following messages from Console Window in ST32CubeIDE

Please fix this....

 

-------- Console Messages -----

STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------

 

Log output file: C:\Users\selly\AppData\Local\Temp\STM32CubeProgrammer_a16720.log
ST-LINK SN : 003200163532510E31333430
ST-LINK FW : V3J12M3
Board : STM32U5A9J-DK
Voltage : 1.79V
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 003200163532510E31333430
ST-LINK FW : V3J12M3
Board : STM32U5A9J-DK
Voltage : 1.79V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x481
Revision ID : Rev C
Device name : STM32U5xx
Flash size : 4 MBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0x92
Debug in Low Power mode enabled

-------------------------------------------------------------------
Choose flashing speed for Cortex M33 series.(default speed=Reliable)
-------------------------------------------------------------------

 

Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a16720.srec
File : ST-LINK_GDB_server_a16720.srec
Size : 47.30 KB
Address : 0x08000000


Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 5]
Download in Progress:


File download complete
Time elapsed during download operation: 00:00:00.544

 

Verifying ...

 


Download verified successfully


Shutting down...
Exit.

---

 

 

    This topic has been closed for replies.

    2 replies

    ST Employee
    September 9, 2023

    Hi @Sellyette ,

     

    How are you programming your Discovery board, through STM32CubeProgrammer or STM32CubeProgrammer_CLI?

     

    Did you check that both NRST signals (between STLINKV3 and the STM32U5) are connected?

     

    Thanks in advance,

    Aime

    SellyetteAuthor
    Explorer
    September 10, 2023

    First of all, thank you for your answer.

    I use STM32U5A9J-DK, As you know, It is completely assembled evaluation board.

    I did not any other modification.

    Thank you for your help.

    Explorer II
    November 13, 2023

    Hi

    Just a thought -- your situation may be different.

    I was using my Laptop's USB port to power up the STM32U5A9J-DK and I recall running into similar issues. I reviewed the specifications and there it stated that the DK board requires 500MA for it to properly enumerate over the USB interface. I updated my USB cable to something that was able to sustain the 500mA draw from the laptop (and I also added a powered USB hub so that the current is not limited) and I was able to get around the issue of not being able to connect to the design kit.