Skip to main content
Visitor II
November 28, 2019
Question

P-L496G-CELL02: No Welcome Message in Tera Term, no Voucher Cod

  • November 28, 2019
  • 3 replies
  • 769 views

Hi! I wanted to start with P-L496G-CELL02. I followed all instructoins from website (video), I have Drivers etc. installed, but in Tera Term I have not got any welcome messages, even my Voucher Cod, so I can't add a new board on https://stm32-c2c.comI have connected the Board with STLink in Tera Term, but Tera Term does realy nothing else.

I have allready did a many tries, different settings but nothing helps...

    This topic has been closed for replies.

    3 replies

    ST Employee
    November 28, 2019

    ​Do you still have the original FW or do you flash a new FW on the STM32 board ?

    If it is still the original FW does UART speed is 9600 ?

    Visitor II
    December 2, 2019

    Hi! It is still the original FW, speed is 9600, but actually I have allready tried the other UART speeds, too, and I tried many different settings, different version of Tera Term, etc. With STM32CubeProgrammer I can read (by Memory & File edition), that the Welcome Message is on the board, but by Voucher Code I can see just %s.

    I followed the instructions from https://www.youtube.com/watch?v=b2-37F7wcaI . I use Windows 10 64bit. I have Java 64bit and 32bit, too.

    Anyhow I want to get this Code to test all this featrures of the Board and the Cloud system etc., but actually I have an own SIM Card, too, so it has to work anyway without this Code, too. Could you link my maybe a User Manual about how to get this boad easy to work with my own SIM Card?

    Thanks a lot!

    Super User
    December 2, 2019

    .