Placing a TFT touchscreen on the B-U585AI-IOT02A Evaluation board.
I have recently purchased the B-U585AI-IOT02A Evaluation board for a project and was surprised to see it had Arduino UNO compatible connectors on one side. Since a while ago I had bought some TFT touch screen shields from Adafruit, I was wondering if I could add this touch screen to the Eval board. Has anyone done such a thing, using bare metal, FreeRTOS, or Azure/ThreadX? Note: Elegoo has a very inexpensive (~$16.00 U.S.) TFT touch screen shield available on Amazon, too, which is probably similar to the Adafruit board.
Any advice of project setup, compatible library code, etc. would be appreciated. I would post my own progress on this here, if any. Thanks!
Rufus