Skip to main content
Visitor II
September 22, 2020
Solved

Position of pinout

  • September 22, 2020
  • 3 replies
  • 2229 views

Hy, I have a Nucleo STM32H743ZI2 and I need use the pin PF_1 and pin PF_2. I search in pinout and the position of PF_1 and PF_2 doesn't correspond in the board, in that position figure (NC)

Tanks!

    This topic has been closed for replies.
    Best answer by TDK

    The schematic is correct, the silkscreen is not. I have that same board and just probed it.

    It's not the first time there have been errors in the silkscreen.

    Not there's also different revisions of the board. Mine is MB1364C. The one in the user manual is MB1364E and has the correct silkscreen.

    3 replies

    TDKAnswer
    Super User
    September 22, 2020

    The schematic is correct, the silkscreen is not. I have that same board and just probed it.

    It's not the first time there have been errors in the silkscreen.

    Not there's also different revisions of the board. Mine is MB1364C. The one in the user manual is MB1364E and has the correct silkscreen.

    SRivi.1Author
    Visitor II
    September 22, 2020

    Tanks you!!

    ST Employee
    September 30, 2020

    Hi @SRivi.1​ 

    Can you please provide me the board reference?

    SRivi.1Author
    Visitor II
    September 30, 2020

    Hy @Bouraoui Chemli​ 

    I'm not sure If I understand correctly, what do you mean with board reference? I can send you the photo of the board.0693W000004II3yQAG.jpg0693W000004II3tQAG.jpg

    ST Employee
    October 7, 2020

    Hi @SRivi.1​ 

    I checked the PCB layout for MB1364C (your board) and MB1364E and confirmed the typo. On MB1364C, PF1 and PF2 are labelled as "NC" whereas they are well connected to the STM32H7. On MB1364E this issue has been corrected and now the labels are OK. Since this problem has been corrected on the latest PCB revision, there will not be any action on the MB1364C board. However, I raised this internally, this typo will be mentioned in the User Manual documentation so that the customers can be aware about it.

    Thanks