Power through STLINK-V3MINI/MODS USB connector?
I have a STM32H750 board and I have been able to do the debugging by powering the board through STLINK-V2. I have some other boards, where the 3V3 or 5V through STLINK-V2 is not used and the power is often through an USB connector.
My STM32H750 board has the USB connector but the 5V power is not connected. Is there any way, that I could tap on the 5V power in the USB connector on STLINK-V3MINI/MODS board.
PS. I do prefer the MODS over MINI to allow easy building of custom cables for different use cases. The manual soldering of wires to 0.05 pitch was a new experience, but not a major challenge. A hot shrink tube is protecting the soldered wires.
PPS. I really like the small size of V3MINI/MODS. The V3SET has a nice functionality, but it is bulky and requires 3D printed case in real life.