Powering a daughterboard from a STM32F4 Discovery Board for prototype
I need 16 DAC outputs for my project. I was planning on using Texas Instrument's DAC8168IAPW over I2C and making a daughter board to connect to the Disco board. I also plan on adding an IC to drive LEDs. Do I power the daughterboard using the Disco board's voltage regulator or should I power the daughterboard with it's own supply? Do I connect a wallwart to the Dicso board even though I still have it connected to my USB port? I don't want to damage my USB port or the board.