Skip to main content
Explorer
January 25, 2024
Question

Problem BLE Extension board

  • January 25, 2024
  • 1 reply
  • 829 views

Hello, I am using the NUCLEO-WL55JC2 board with the X-NUCLEO-BNRG2A1 ble extension board. I run the SensorDemo_BLESensor demo code and I can detect my board in the BLE Sensor application In my phone. However, I want to connect a DHT11 temperature sensor but when I connect the VCC pin of the sensor to the +5V or +3V3 on CN6 connector of the extension board I can no longer detect the board in the application. 

In the documentation, I see that that the pins are corresponding : 

LearnCORE_0-1706211464707.png

Do you have any idea of what the problem may be? 

Thanks for your time 

    This topic has been closed for replies.

    1 reply

    Graduate
    February 15, 2024

    Hello, following your post here, it seems that you have solved the issue and can communicate with the BLE-Module with that board, would you share the configurations that you followed to make it work (Advertising) as I get the "Read Static Random address failed" error due to the configurations.


    AElgh_0-1708014051322.png

     

     

     

     

    Thank you