PROBLEM Debug project with external loader
Debug project with external loader
Hi all,
I have a project with an external loader and I didn't succeed to enter to debug and download the hex (sometimes is and sometimes it is not it didn't consistency
i didn't understand if it's the st programmer or
see log :
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\TFS\Software\Projects\RK\source_code\release\code_2024\controlller\1\rks_controller\debug_new\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61244
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
COM frequency = 4000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fdfd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J40S7
Device ID: 0x452
PC: 0x800b380
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.22 V
ST-LINK device status: HALT_MODE
Run external memory initializer
ST-LINK device initialization OK
Stm32Device, pollAndNotify running...
SwvSrv state change: 0 -> 1
Waiting for connection on port 61245...
Waiting for debugger connection...
Waiting for connection on port 61244...
Accepted connection on port 61244...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61244...
GDB session thread running
GdbSessionManager, session started: 1
Warning: Ignoring a '-' sent by client....
Stm32Device, closeDevice() entry
GDB session, device event: 5
Stm32Device, pollAndNotify stopped
Stm32Device, closeDevice() exit
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
Log output file: C:\Users\nbitan\AppData\Local\Temp\STM32CubeProgrammer_a25876.log
Warning: Wrong connect parameter: speed=fast
ST-Link Server is running on port : 7184
ST-LINK SN : 50FF6F067788545406291867
ST-LINK FW : V2J40S7
Board : --
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x452
Revision ID : Rev A
Device name : STM32F72x/STM32F73x
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x__
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a25876.srec
File : ST-LINK_GDB_server_a25876.srec
Size : 594368 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 8]
Download in Progress:
�������������������������������������������������� 0%
��������������������� 43%
Error: failed to download Segment[0]
Error: failed to download the File
------ Switching context -----
COM frequency = 4000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fdfd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J40S7
Device ID: 0x452
PC: 0x800b380
ST-LINK detects target voltage = 3.22 V
ST-LINK device status: HALT_MODE
Run external memory initializer
GDB session, device event: 3
GDB session, device event: 1
ST-LINK device status: RUN_MODE
GDB session, device event: 4
GDB session, device event: 4
GDB session, device event: 6
Stm32Device, pollAndNotify running...
ST-LINK device status: HALT_MODE
GDB session, device event: 0
GDB session, device event: 3
GDB session, device event: 1
GDB session, device event: 0
NVIC_DFSR_REG = 0x0000000B
GDB session, device event: 3
GDB session, device event: 1
ST-LINK device status: RUN_MODE