Problem flashing the code onto STM32F4 DISCO board
Hello!
I have installed Keil uVision and STM32 Cube on Ubuntu 18 LTE and when I try to flash the code onto my DISCO board it says that there is no board detected. I have a feel like if ST-Link2 isn't properly installed or maybe there are additional drivers for Linux that are needed in order to flash the code. I'm also running uVision via Wine. When I type usb-device on my Ubuntu terminal, the kernel sees the STM device attached to the machine via usb port.
Thank you!