problem of using USART6 on STM32F769I DISCOVERY kit board
I am using the usart6 port (PC6 and PC7) on a STM32F769I DISCOVERY board to communicate with another STM32F769I DISCOVERY board. I use cubemx generated code "MX_USART6_UART_Init" to initiate the usart6 and use "HAL_UART_Transmit" on sender and "HAL_UART_Receive_IT" on receiver. The problem I have now is the received data shifts one byte to right compared to the send data. Both "HAL_UART_Transmit" and "HAL_UART_Receive_IT" returns with "HAL_OK".
Any thoughts what could be the root cause? Thanks!