PROBLEM: reconnecting a Nucleo-F767ZI with the cut ST-Link.
I'm a STM32 beginner and i'm trying to reconnect a Nucleo-F767ZI with the cut ST-Link. I'm working with ChibiOs and i get the error: target voltage may be too low for reliable debugging. But i get some kind of communication (LD1 shows red and green)
I'm using the SWD Port on the ST-Link and an external 5V powersupply (E5V) and I connected the SRT-Link like this: SWCLK to CN11 pin 15, SWDIO to CN11 pin 13, NRST to CN11 pin 14, VDD_Target to CN11 pin 5. I also detached the Jumpers CN4 on the ST-Link and got the Jumper JP3 to E5V.