Problem to flash external 1,8V board with StlinkV2 Nucleo debugger
Hi,
I have a custom board with a STM32L4 powered at 1.8V. I program it without problems with a STLINK-V3MINIE.
Now I want to program it with the stlinkV2 of the NUCLEO -L4R5ZI-P (I have cut it, removed CN4 and connected pins 1,2,3,4 and 5 to CN5):

I can connect and read the memory, but if I try to program, the flash is erased, but not written and the IDE shows this error:

What could be the problem?
Thank you very much!