Skip to main content
Visitor II
January 16, 2023
Solved

Problem with flashing STM32G070 MCU via i2c after ST link has been used

  • January 16, 2023
  • 2 replies
  • 2213 views

I'm using a STM32G070 MCU which I flash via i2c when the boot0 pin is set to high.

This works fine until I connect a ST-link to the MCU, program it and then disconnect the ST-link again. After that the i2c flash will fail, I have checked the boot0 and reset pin and these are set correctly, but when checking the i2c communication it seems like there is no reply from the boot loader address 0x51.

When I power cycle the MCU the i2c flash works fine again.

I have checked the boot select bit in the user option byte and it looks ok.

Anyone know if this is expected behavior after the ST link has been used or if it might be something I have missed?

    This topic has been closed for replies.
    Best answer by Bubbles

    Hi @ChrisTh.2​,

    it would appear that by connecting the debug interface, you have engaged read protection. That can only be lifted using power cycle, not by a system reset. It's a precaution to prevent reading the system memory (which contains more than just the i2c bootloader).

    BR,

    J

    2 replies

    BubblesAnswer
    ST Employee
    January 17, 2023

    Hi @ChrisTh.2​,

    it would appear that by connecting the debug interface, you have engaged read protection. That can only be lifted using power cycle, not by a system reset. It's a precaution to prevent reading the system memory (which contains more than just the i2c bootloader).

    BR,

    J

    ChrisTh.2Author
    Visitor II
    January 19, 2023

    Ok I didn't know about the read protection, but then it makes sense.

    Thanks for the reply!