Skip to main content
Graduate II
October 15, 2019
Solved

Problem with new ST-Link/V2 Programmer

  • October 15, 2019
  • 3 replies
  • 1027 views

I have a ST-LINK / V2 programmer that I bought 4 years ago and it works perfect. I recently bought two new programmers but none work with the same connections like old programmer. I updated each firmware but it still doesn't work. Has anything changed in the new programmers? In document of ST-Link i haven't seen any change in hardware. my hardware is as followed:

MCU Programmer

SWDIO (PA13)-> SWDIO (Pin 7)

GND -> GND (Pin 20)

3.3V -> 3.3V (Pin 19)

SWCLK (PA14)-> SWCLK (Pin 9)

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    Check you have power.

    You should also connect the board power back to pin 1 or 2 of the ST-LINK to power the buffers.​

    3 replies

    Graduate II
    October 15, 2019

    You should tell on what system you work and what exactly does not work?

    SlhAuthor
    Graduate II
    October 15, 2019

    My system is Windows 7 and error is so:

    0690X00000AqN7JQAV.jpg

    and with SW4STM32 IDE, i have this error:

    0690X00000AqN8CQAV.jpg

    Graduate II
    October 15, 2019

    Check you have power.

    You should also connect the board power back to pin 1 or 2 of the ST-LINK to power the buffers.​

    SlhAuthor
    Graduate II
    October 15, 2019

    Thank you! It works, but I'm confuse why my old programmer works without connection to Pin 1 or 2 of programmer. Could it be fake?

    Graduate II
    October 15, 2019

    Well a lot of the fake/clone devices lacked the buffering that the original design had, so worked due to the more direct mcu-to-mcu connectivity