Problem with the nRST pin in a STM32L021K4
I already read this post with no success: https://community.st.com/s/question/0D50X00009Xka0fSAB/problem-with-the-nrst-pin-in-a-stm32f100cbt6
I tried to design a simple board with a STM32L021K4 and to program it with a STLINK-v3 MINI. I got the following error message:
Error in initializing ST-LINK device.
Reason: Target held under reset.
(You can see the full logs attached, as well as the schematics)
I measured the nRST pin, and it's about 0V. I measured VDD and VDDA, and they are at 3.3V. BOOT0 is connected to GND.
I added a 100nF capacitor from nRST pin to the ground and I tried to short the inductor of the VDDA filter.
Did I miss something obvious? Did I burn something?
Do you have any idea before I waste another PCB?