Skip to main content
Visitor II
October 11, 2018
Question

Problems with flashing into Nucleo32-l432kc

  • October 11, 2018
  • 1 reply
  • 595 views

Hello,

I have Nucleo32-l432kc board. When I am trying to run the ST-Link upgrade application it is showing ST-Link device not detected even though I connected the board. Later, when I am trying to flash the code it's not working, I assume because of the earlier issue.

Could anyone please help me with this problem?

Thanks in advance!!!!!!!

    This topic has been closed for replies.

    1 reply

    Graduate II
    October 11, 2018

    Make sure you can see the ST-LINK device in Device Manager.

    Don't have the ST-LINK open in a debugger or running code. Press the reset button, and get the update utility to refresh.