Problkems with NUCLEO-H743ZI2 onboard ST-Link
Hello,
I bought a NUCLEO-H743ZI2 board.
When I plugged it in for the first time, I was able to flash it after two or three attempts (ST-Link was often not recognised).
But now the STM32CubeProgrammer does not recognise the ST-Link at all (I have tried more than 20 times with different USB cables).
When I plug the board into the PC, I get a virtual COM port "STMicroelectronics STLink Virtual COM Port (COM23)" in the device manager.
So the ST-Link seems to communicate. But the programmer still does not recognise it.
What could be the reason?