Program does not execute after resetting power
Hello,
We have developed a custom board having STM32F746NGHx MCU based of the design of the STM32F746G-DISCO board.
We are using ST-Link Utility and ST LinkV3-SET Debugger in JTAG mode to flash.
The board gets flashed and the program is executed after flashing is complete and the display (TFT _ LCD) shows desired output.
But, if the board is reset, the program does not execute and the display shows garbage.
But it executes again only if the STLinkV3-SET Debugger is disconnected and reconnected to the PC.
Please advice on the issue.
Thanks,
Ameya