(programmed) STM32F030 stucks in the startup (xx.s ) forever. defective batch ??
the hole batch of F030C6T6 has same behavior :
can access with ST-Link , program, verify - all ok. read core registers, option bytes...ok.
but then no program start ! chip stays in startup here:
10 tested boards ihave identical behavior. chips coming from PCB assembler , as usual.
I replaced one with a (suspect source , from aliexpress dealer) F030 , then board running as it should.
- can i do anything, to get these boards running?
- if chips have all same defect, how is it possible to passing the wafer test ??