Skip to main content
Visitor II
May 5, 2021
Question

Programmer for Steval-IDP004V2 with the help of st link v3 mini

  • May 5, 2021
  • 1 reply
  • 563 views

Hallo Support Team,

i have a "STEVAL-BFA001V2B" kit containing

  • STLINK-V3MINI debugger/programmer for STM32 and STDC14 flat cable. 
  • One adapter for ST-LINK programming and debugging tool - STEVAL-UKI001V2.

and i had also the  STEVAL-IDP004V2 master board which has a ST Link V2 programmer, is it possible to use ST Link v3 mini for programming/Debugging " STEVAL-IDP004V2" , do i need another adapter for st link V2 20 pin?.

Thanking you.

Kind Regards,

Govil

    This topic has been closed for replies.

    1 reply

    Super User
    May 5, 2021

    You'll need an adapter since the STLINK-V3MINI only has the 0.050" pitch cable connector, but the STLINK-V3MINI can be used as a programmer.